Fast Inductive Load Turn-off (Fast Demagnetization)
Traditionally, inductive loads (such as a solenoid drive) use a free-wheeling diode in
parallel with the load to discharge stored energy to reach the Off status (zero
current). This process is called Demagnetization.
The PointMax high-speed counter/SSI module has the fast inductive load turn-off feature.
If the inductive load is within the module's specified inductance and current rating,
then no free-wheeling diode is required. Demagnetization is performed faster when
compared to using an external free-wheeling diode. For the module inductance and current
rating specifications, see the PointMax I/O System Specifications Technical Data,
publication 5034-TD001.
There are two possible demagnetization scenarios. Typically, inductive load
demagnetization happens as illustrated in Demagnetization Example 1. In this scenario,
demagnetization happens entirely through the high-side active clamp switch and the
output voltage is at a negative voltage of (SA voltage + VCL) during the demagnetization
phase.
Demagnetization Example 1
However in some situations, demagnetization happens as illustrated in Demagnetization
Example 2. The demagnetization happens through the combination of high-side active clamp
switch and low-side switch. The output voltage switches between a negative voltage of
(SA voltage + VCL) and approximately 0 volts during the demagnetization phase.
Demagnetization Example 2
Provide Feedback