Estimate memory requirements offline for controllers with divided memory
When a project changes on a controller with divided memory, use the
Estimate
button on the Capacity
tab of the Controller Properties
dialog box to see the estimated memory usage and remaining available memory.
IMPORTANT:
This procedure applies to the CompactLogix 5370, ControlLogix 5570, Compact GuardLogix
5370, and GuardLogix 5570 controllers.
Some controllers, for example Compact GuardLogix 5380, CompactLogix 5380, CompactLogix
5480, ControlLogix 5580, GuardLogix 5580, and ControlLogix 5590 controllers, store all
elements in one common area and the data values are automatically updated when the project
changes.
To estimate controller memory requirements offline:
- On theOnlinetoolbar, click theController Propertiesicon.
- On theController Propertiesdialog box, click theCapacitytab.
- (optional) InMemory Optionbox, select the controller that has the correct memory size.
- View the memory information that is available since the last estimate.
- SelectEstimateto re-estimate the amount of controller memory required for the project.
- SelectOK.
Provide Feedback