Linear command
Choose this command to change the selected cam segments to linear type. When all cam segments are linear, this command is disabled.
TIP:
Selecting a cam point also
selects the cam segment which follows it, so that both the cam point and cam segment are
highlighted.
Provide Feedback