Complete Hookup Diagnostics and Auto Tuning
After you add and configure your modules and axes, you can download your program. After going online, you can complete hookup diagnostics and auto tuning.
To run hookup diagnostics and auto tuning
- To download your program, from theCommunicationsmenu, selectGo Online.TIP: Your program can be a blank program, but it must include complete configuration information for all your modules and axes.
- Under theI/O Configurationfolder, right-click the first motion module.
- SelectProperties.
- Decide on the appropriate button to select:If:Then:You assigned your axis to channel 0Select the
button next to the Channel 0 fieldYou assigned your axis to channel 1Select the
button next to the Channel 1 field - Select theHookuptab.
- Run the hookup diagnostics. For more information about hookup diagnostics, see the ControlLogix Motion Module User Manual.
- Select theTune Servotab.
- Run auto tuning. For more information about auto tuning, see the ControlLogix Motion Module User Manual.
- When diagnostic testing and auto tuning are complete, selectFinish.
- For each axis, repeat steps 4 through 9.
- For each module, repeat steps 2 through 11.
Provide Feedback