Corrected anomalies
This list identifies the anomalies that are corrected in the Logix Designer application
version 38.00. Use the identification information provided in parentheses to track the anomaly
in future releases or for reference when receiving assistance from Customer Support with a
related issue.
General
Tag of Datatype UDT with bit overlay cannot be changed by any code (5108016)
A tag with a user-defined datatype (UDT) that contains bit overlay members and
single-dimension array members cannot be changed/written by any code. Although you cannot
create bit overlays in the Logix Designer application, you can add them through an import.
This anomaly first identified in version 28.00.
This anomaly corrected in version 38.00.
Toggle Inline Value Display Feature Causes Slow Software Performance (3323352)
Using the
Toggle Inline Value Display
feature in a Structured text routine can slow
software performance when toggling the value display on or off. After many repeated toggles of
the value display, the software may become unresponsive.This anomaly first identified in version 31.00.
This anomaly corrected in version 37.00.
Logix Designer version 36.00 installer fails to install AOP Core when GuardLink EIP
Scanner AOP is already installed (3185534)
When a Guardlink EIP Scanner 432ES AOP version 1.00.34 is already installed on your Logix
Designer workstation and you attempt to install version 36, installation errors occur and the
installer fails to install AOP core files.
To work around this issue, uninstall the GuardLink EIP Scanner AOP from your Logix Designer
application before installing version 36.00. For more information, see
this Knowledgebase article
.This anomaly first identified in version 36.00.
This anomaly corrected in version 38.00.
Error Creating Signature History when Importing and Overwriting an Existing AOI
(4169419)
- You import a signed Add-on Instruction (AOI) with a signature history.
- The option to overwrite an existing AOI without a signature history is enabled.
- The existing AOI’s signature history is blank.
To resolve this issue, add entries to the signature history of the existing AOI.
Then retry the import process.
This anomaly corrected in version 38.00.
Application fails to upload when structured text comments contain specific combination of
characters (4006663, 4036071, 4036072, 4036074)
For the CompactLogix 5380 Controller, CompactLogix 5480 Controller, and ControlLogix 5580
Controller, when a Structured Text routine includes a comment with nested square brackets "[]"
followed immediately by a greater-than ">" character (example
//[commen[t]]>
) the
Logix Designer application fails to upload from the controller and displays Error: Logic
reconstruction data may be corrupted.
An example of problematic comment syntax that causes the upload failure is:
//[commen[t]]>
This issue impacts Structured Text routines in CompactLogix 5380 Controller, CompactLogix
5480 Controller, and ControlLogix 5580 Controllers.
To resolve this, adjust the comment syntax by reducing the number of square brackets or by
removing the greater-than character at the end of the comment. For example, the following
syntax allows the upload to succeed:
//c[ommen[t]]
//[comme[n]t]>
This anomaly first identified in version 33.00.
This anomaly corrected in versions 35.03, 36.02, 37.01, and 38.
A Message Instruction (MSG) Cache Connections option is not reflected properly while
offline (3995824)
If a Message instruction’s Control tag is defined as program-scoped and the options in the
Message configuration > Communication tab for Connection is checked and Cache Connections is
unchecked, going offline the ACD file will erroneously indicate that both of these options are
checked. Performing a save of the application while online will not correct this.
If the offline ACD file is downloaded to the controller, message instructions that have the
Cache Connections checkbox unchecked will now have them checked.
This issue only affects 5380, 5480 and 5580 controllers.
To work around this issue, in the application code use an OTU instruction to reset the EN_CC
bit in the message control tag.
This anomaly first identified in Logix Designer version 32.00.
This anomaly corrected in version 38.00.
High CPU and Memory Usage in Structured Text (4004601)
The Logix Designer application experiences elevated memory & CPU usage and can go into a
“Not Responding” state when inline values are enabled in Structured Text.
This anomaly first identified in version 33.00.
This anomaly corrected in version 38.00.
Provide Feedback