Backing Tag Properties dialog box - Parameters tab settings

The following table describes the parameters on the Backing Tag
Properties
dialog box -
Parameters
tab.
Parameter
Description
Input/Output Row Header
An
I
at the start of a row indicates and Input parameter; an
O
indicates an Output parameter.
Vis
Select the check boxes in this column to determine which parameters are visible on the function block.
If the parameter is wired to another parameter, the check box will be selected, and can not be cleared because the parameter must be visible on the block.
Name
The name of the parameter. Information in this column is read-only.
Value
Displays the current value of the parameter. Values in this column are displayed according to the display style of the block tag’s data type.
If the parameter is wired to, the value column will be read-only, and the value cannot change. If you modify this value while online, it has an immediate effect.
Type
Displays the data type for the parameter. Information in this column is read-only.
Description
Displays the description of the parameter. Information in this column is read-only.
Insert Instruction Defaults
Resets the
Vis
and
Value
columns to the user-stored default values.
Insert Factory Defaults
Resets the
Vis
and
Value
columns to Factory default values.
Save Instruction Defaults
Enables storing the current values as the instruction defaults.
Status
Displays status information for blocks containing status bits. If none of the status bits are set, an
OK
message appears in this field. Otherwise, a list of the status bits that are set appears here. This list is comprised of the parameter names associated with the status bits, and typically explain which parameters were configured with invalid values.
Sort Parameters
Select this check box to sort the parameters alphabetically. Sort the names in the
Name
,
Type
, and
Description
columns by double-clicking on the column header cell. Subsequent clicks on the column heading alternate the sort between ascending and descending values. The check box is not selected by default.
Execution Order (only applicable to Function Block Diagrams)
Displays the block's execution number if the routine is in a verified state. If the routine is not yet verified, a
Routine not verified
message appears. Note that this item is read-only.
Never display description in a routine (only applicable to Function Block Diagrams)
Select this check box to disable the description from displaying in the routine.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal