Non-regen Converter Axis Behavior

When the Motion Device Axis Object is associated with a CIP Motion Non-regenerative Converter, the Active Control state diagram reduces to the following diagram. Shaded regions show mapping of Axis States to corresponding Identity Object states. State transitions ending on shaded boxes can transition to any axis state within the box.
Motion Device Axis Object State Model (Converter)
TIP: *Specific Standby state after a fault reset is determined by applying Fault Reset State Transition Precedence rules.
Valid transitions for the Axis State Model of a CIP Motion Non-regenerative Converter axis are explicitly defined in the following table:
Current State
Event
Conditions
Next State
Off
Power Up
Self Test
Self Test
Self Test Complete
Initializing
Initializing
Initialization Fault
Major Faulted
Initializing
Initialization Complete
Pre-Charge
Shutdown
Major Fault
Major Faulted
Shutdown
Shutdown Reset
Pre-Charge
Start Inhibited
Shutdown
Shutdown
Start Inhibited
Major Fault
Major Faulted
Start Inhibited
Brake Slip Exception Major Fault
SI = 0
Aborting
Start Inhibited
Inhibits Cleared
Pre-Charge
Pre-Charge
Start Inhibit
Start Inhibited
Pre-Charge
Shutdown
Shutdown
Pre-Charge
Major Fault
Major Faulted
Pre-Charge
Bus Up
Running
Major Faulted
Fault Reset
Shutdown = 1
Shutdown
Major Faulted
Fault Reset
Shutdown = 0
Pre-Charge
Major Faulted
Reconnection
Initializing
Running
Not Bus Up
Pre-Charge
Running
Shutdown
Shutdown
Running
Major Fault
Major Faulted
Any State
Connection Close
Initializing
Any State
Connection Loss
Major Faulted
Axis Test Mode
L5K_RM003_OperationalDiagramAxisTestMode_3_v36
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back simulate these transitions of a CIP Motion Non-regenerative Converter axis.
Current State
Event
Conditions
Next State
Axis Test Mode Support
(Test Mode Configuration)
Off
Power Up
Initializing
Controller Loop Back: V35
Initializing
Initialization
Complete
Running
Controller Loop Back: V35
Running
Shutdown
Shutdown = 1
Shutdown
Controller Loop Back: V35
Shutdown
Shutdown Reset
Shutdown = 0
Running
Controller Loop Back: V35
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal