Must specify a folder to create project in.

When creating a new controller, enter the directory to store the project file. The project files saves to the specified directory with the same name as the controller and has an .ACD file extension.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal