New Parameter or Tag dialog box parameters
Use the
New Parameter or Tag
dialog to create program parameters or tags. The table describes the parameters in the dialog. Parameter | Description |
Name | Used to enter a name for the tag. If you are creating a new program parameter from a language editor, and the parameter is from another program, the tag name appears in the Name box. |
Description | Used to enter a description for the tag. |
Usage | The Usage value for the tag or program parameter.
|
Type | Used to select an Alias , Base , Produced , or Consumed type tag. There are additional considerations for produced and consumed tags.
There are several tag requirements for producing data.
|
Connection | Connection is available when you set Type to Produced or Consumed . Connection defines the consumed or produced tag.
IMPORTANT:
Set up only one consumed tag to get data from the same producing tag in another controller. Setting up more than one consumed tag can result in unpredictable controller-to-controller behavior.
|
Alias For | Used to select the base tag and qualifier that the tag references. For an Add-On Instruction definition, only Input and Output tags can alias Local Tags; Local Tags and InOut tags cannot alias another tag. The controller must be offline before you can make changes to this box. |
Data Type | Used to select the type of tag to create. Used the to open the Select Data Type dialog, and select a data type. These data types require additional configuration:
For alias tags, this box is read-only as the data type of the alias tag is defined by the base tag. These tags can only be used in controller scope and do not support arrays:
There are additional considerations for data types that are used with safety tags.
The following data types cannot be used when creating Safety tags: AXIS_CONSUMED, AXIS_GENERIC, AXIS_GENERIC_DRIVE, AXIS_CIP_DRIVE, AXIS_SERVO, AXIS_SERVO_DRIVE, AXIS_VIRTUAL, MOTION_GROUP, MESSAGE, COORDINATE_SYSTEM, ALARM_ANALOG, ALARM_DIGITAL, and MODULE data types. The software prevents the direct creation of invalid tags in a safety program. In the event that invalid tags are imported, they cannot be verified. In Safety programs, the Logix Designer application also prevents:
|
Parameter Connection | Used to select a single connection for the parameter. If you need to make multiple connections, select the Open Parameter Connections check box. When you click Create , the Configuration Connection dialog box opens and you can view and configure connections for the parameter. |
Scope | Used to select the scope in which to create the tag. Select controller scope or one of the existing programs on the controller. If you are creating a new program parameter from a language editor, and the parameter is from another program, the program name appears in the Scope box. |
Class | Indicates whether the tag is a Standard tag or a Safety tag. This value appears for Safety applications only. |
External Access | Used to select the access allowed to the tag from external applications such as HMIs. The available options include:
|
OPC UA Access | Used to select the level of access that external OPC UA clients have to tags. The available options include:
|
Style | The display format for this data type. Use these settings:
|
Constant | Select the Constant check box to prevent executing logic from writing values to the associated tag or parameter. If a logic routine tries to write to a constant tag, the routine will not verify. The Constant check box is not available for all tag types.Tip: You can use the Data Monitor dialog box to write values to the parameter. The Value boxes in all other browsers and language editors are disabled when the tag is a Constant tag. Changes made to the values of constant tags are recorded in the Controller Log for future reference. |
Sequencing | Enables the tag or parameter visible on the FactoryTalk Batch server to be visible. Only tags and parameters on which Usage is set to Input or Output can be used by a sequence. |
Open Configuration | Enables a configuration wizard or dialog box to open after you select Create .The Open Configuration check box is available for only specific data types and is not available for program scope tags that are set to InOut for Usage . |
Open Parameter Connections | Enables the Configuration Connection dialog to open after you select Create . |
Provide Feedback
to open the