About external access to public and private data

The
External Access
property setting allows you to specify the level of access (Read Only, Read/Write, or None) external applications and devices have to tags. These external applications and devices include:
RSLinx® Classic
and
FactoryTalk® Linx™
Other Logix controllers
PanelView
PLC/
SLC
controllers
FactoryTalk Historian
3rd party software
The following table describes
External Access
settings:
External Access setting
Description
Read/Write
External applications and devices have full access to the tag and can therefore read and change the tag's value.
Read Only
External applications can read, but cannot change, the tag's value.
None
External Applications cannot read or change the tag's value.
IMPORTANT: The
Logix Designer
application has full access to all tags, regardless of their
External Access
setting.
External access is configured when you create a new tag or data type. After you create a tag, you can modify the tag's
External Access
setting like you would any other tag attribute.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal