Create an Advanced SVG Image object

Add an Advanced SVG Image object representing a conveyor and dynamically link its chassis representation to the alarm.
Prerequisites
Download and extract the SVG 1.2 Tiny image.
  1. To create an Advanced SVG Image object
  2. Create the image object:
    1. In
      Project view
      pane, right-click
      MainWindow (type)
      and select
      New
      Drawings
      Advanced SVG Image
      .
    2. Hover-over the image, select
      Edit
      , and enter
      ConveyorImage
      .
  3. Configure the image object:
    1. Double-click the empty image
      Image placeholder
      on the canvas.
    2. Select
      Import file(s)
      and in
      Import file(s)
      , select the file to import and then choose
      Select
      .
    3. Under
      SVG Element Properties
      Property1
      , set
      ID
      value to
      ConveyorChassis
      .
    4. Create a complex dynamic link between
      Value
      and
      ConveyorChassisMalfunctionAlarmVariable
      with the use of a conditional converter.
      True value
      #f51616
      False value
      #000000
      Condition DynamicLink
      ProjectName
      Model
      ConveyorChassisMalfunctionAlarmVariable
      For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.