Deploy a FactoryTalk Optix Application

Rockwell Automation
target devices automatically run
FactoryTalk Optix Applications
upon deployment. Devices that do not have the update service installed or have the runtime application transferred manually require you to start the application manually on the device or configure the application for automatic startup.
Use
FactoryTalk Optix Studio desktop editor
to deploy to either local or remote devices. Use
FactoryTalk Optix Studio web editor
to deploy to remote devices only.
FactoryTalk Optix Studio
uses
FactoryTalk Remote Access
to deploy to remote devices.
IMPORTANT: If a
FactoryTalk Optix Application
is already running on a target device, deploying another
FactoryTalk Optix Application
stops and removes the other application.
Prerequisites
  • Configure the presentation engine for the mode in which you will be running
    FactoryTalk Optix
    .
  • Confirm that
    FactoryTalk Optix Application Update Service
    runs on the target device.
    IMPORTANT: To operate correctly when running as an application,
    FactoryTalk Optix Application Update Service
    requires the TCP port 49100 to be reachable and a valid username with a configured password.
  • Confirm that the target device has a valid license.
    IMPORTANT: If the target device is not licensed,
    FactoryTalk Optix Applications
    run in the demo mode and stop automatically after 2 hours.
  • Configure a device.
    IMPORTANT: Configure either a local or remote device. To configure a local device, see Manage client devices. To configure a remote device, open
    FactoryTalk® Hub™
    and access
    FactoryTalk Remote Access
    . In FactoryTalk Remote Access Online Help, see
    Domain view
    and scroll to
    To add a device
    . The remote device must also have the
    FactoryTalk Remote Access
    Runtime client installed and configured. In FactoryTalk Remote Access Online Help, see
    Client configuration
    .
  1. To deploy a
    FactoryTalk Optix Application
  2. Select the configured device.
    For more information, see Select a client device.
  3. If you selected a remote device, you must first establish a VPN connection to that device. Select
    VPN
    or a remote desktop connection by selecting
    Remote Desktop
    .
  4. Select
    Run
    .
  5. Enter the user password for the target device and select
    OK
    .
  6. To stop the
    FactoryTalk Optix Application
    on the target device, select
    Stop
    .
The application on the target device stops.
NOTE: To detach FactoryTalk Optix Studio from the target deice, close the Output pane in
FactoryTalk Optix
. The application continues to run on the target device but 
FactoryTalk Optix
is no longer connected so messages no longer appear in the Output pane.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal