Delete a connection to a program parameter

Delete a connection to a program parameter

Delete a connection to a program parameter to stop passing the data from the parameter into and out of the program for a controller tag, device tag, or other program tag.
  1. On the explorer bar, select System Icon
    System
    and then select the program.
  2. In the
    System
    title bar, Select Tags Icon
    View tags and parameters
    . The Tag Editor opens.
    TIP: To open the Tag Editor, you can also right-click the program and select
    Tags and parameters
    .
  3. On the Tag Editor, select the parameter.
  4. In
    Properties
    , select
    Connections
    .
    TIP: If
    Properties
    does not open, in the pane bar, select Properties Icon
    Properties
    .
  5. Next to the connection to delete, select Delete Icon
    Delete
    .
  6. (optional) To undo the deletion, in the toast, select
    Undo
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal