Manage devices
Add, remove, and assign devices from a project or view device profiles to configure how devices communicate between controllers and hardware.
FactoryTalk Design Studio Copilot and devices
FactoryTalk Design Studio Copilot offers these prompts for devices.
- Search for devicesPrompt:Search for ControlLogix I/O modules.FactoryTalk Design Studio Copilot response: If no devices match that search criteria, a message appears stating no devices match.
- Create devices using catalog numberPronpt:Create a device with catalog number 1756-L83E, name CTRL, and assign it to Slot 0.FactoryTalk Design Studio Copilot response: A warning that FactoryTalk Design Studio Copilot cannot complete this prompt if one of these scenarios exist:
- The catalog doesn’t exist or is not supported.
- The name is already used or is invalid.
- The assignment is invalid
- Update device propertiesPrompt:Update the CTRL firmware revision to v32.11.FactoryTalk Design Studio Copilot response: A warning that FactoryTalk Design Studio Copilot cannot complete this prompt if one of these scenarios exist:
- The device does not exist.
- The property does not exist.
- The Property value is invalid.
- Update device assignmentPrompt:Update the assignment of DigitalInputModule to Slot 3FactoryTalk Design Studio Copilot response: A warning that FactoryTalk Design Studio Copilot cannot complete this prompt if one of these scenarios exist:
- The device does not exist.
- The assignment target is invalid.
- Delete DevicesPrompt:Delete the 1756-IA16 digital input module.FactoryTalk Design Studio Copilot response: A warning that FactoryTalk Design Studio Copilot cannot complete this prompt if one of these scenarios exist:
- The device does not exist.
- More than one device type is in the project. FactoryTalk Design Copilot provides a list for you to choose which one to delete.
Find information about FactoryTalk Design Studio Copilot prompts for:
Provide Feedback