Network paths
The network path specifies the target network for status monitoring in an
IntelliCENTER
lineup. You
must provide all network paths within a lineup before the lineup starts status monitoring.
After creation, modify network paths in the Edit Network Paths
tab. Launch the
Set Network Path
or Edit Network Path
tab from the:
TIP:
If you start monitoring and all network paths have not been set, the
Set Network Path
tab opens automatically for you to set the remaining paths. To communicate with a controller, Add a VPN driver.Provide Feedback