Enable FactoryTalk Design Studio Copilot - Project Access
FactoryTalk®
Design Studio™
Project Access
is a setting related to FactoryTalk Design Studio
Copilot. This setting controls FactoryTalk Design Studio
Copilot's ability to read and write data from a FactoryTalk Design Studio
project and is enabled by default. The
Project Access
setting can be disabled for a project, preventing
FactoryTalk Design Studio
Copilot from accessing the project content. When disabled, FactoryTalk Design Studio
Copilot cannot generate project insights or new project code. This setting applies to the
currently open project for your user only. It will not impact other users.To enable FactoryTalk Design Studio Project Access
- SelectFile > Options.
- SelectCopilot.
- InCopilot, toggleProject AccesstoOn.
See FactoryTalk Design Studio Copilot
for more information.
Provide Feedback