Change the setpoint of a timer step
You can change the setpoint of a Timer step whether or not it is currently active and regardless of its state.
- In the Batch List view, double-click the batch that contains a Timer step. The batch opens in the Procedure view.
- Select the Timer step in the SFC or Table view, and then click theDetailsbutton. ThePropertiesdialog box opens.
- Select theParameterstab to view the Hold Behavior, Setpoint (COUNT_DOWN timers only), and Timer Type for the selected Timer step.

- Double-click anywhere in the SETPOINT row. TheChange Parameter Valuedialog box opens.

- Type a new setpoint value in the Value box, and then clickOK.The value entered must be within the displayed minimum and maximum values for the parameter. If the value is between the minimum and maximum values when you clickOKthe new value is sent to the Timer step. If the value is not between the minimum and maximum values, an error message requests "Please enter a value between the configured Minimum [Minimum Value] and Maximum [Maximum Value] values". ClickOKto enter a new value.
- ClickOKto close thePropertiesdialog box and apply the change.
Provide Feedback