Manual phase binding
Manual phase binding is the process of binding a unit (equipment phase), or rebinding a previously bound unit, to a step within a control recipe without being prompted to do so. Manual binding must be performed from within the Procedure view (Table or SFC mode).
The following criteria must be met in order to perform manual phase binding:
- The step is associated with a unit class in the recipe’s equipment requirements.
- The step represents the highest recipe level wholly contained within the unit. (For example, one step in the recipe represents a unit procedure that is associated with the pre-mixer unit class, while another step that is associated with the same pre-mixer unit class is an operation. As long as the balance of the manual binding requirements are met you can manually bind the unit procedure, but not the operation, since the unit procedure is the highest recipe level associated with the unit.)
- The step is inactive or has a binding status of BINDING.
- More than one legal binding choice exists for the unit that is associated with the step.Tip:All other steps within the recipe that are associated with the same unit alias are bound to the same unit. (SeeCreate a procedurein thefor information about unit alias.)FactoryTalk Batch Recipe EditorUser Guide
- In the Batch List view, double-click the batch that requires binding. The Procedure view opens.
- To bind a unit to a step, you must select the unit procedure in either the SFC or Table. If the control recipe was created from an operation or unit procedure, then select the parent level. If the manual binding criteria was met, theBindcommand button is enabled.
- Click theBindcommand button. TheBinddialog box opens with a list of legal binding options.

- Select the appropriate binding type:
- Operator Prompt –When the batch is started and the bound unit is encountered, a message to "Bind Unit Alias" displays in the Instruction view. Select the appropriate item from the list, and then click theOK(orSubmit) button.
- First Available –When more than one unit fits the recipe criteria,eProcedurewill select the first available unit.
- Specific Unit –When more than one unit fits the recipe criteria, you can select which unit to use for the batch.
- If you selectedSpecific Unit, select the specific unit to bind and clickOK. You are returned to the Procedure view. If you selectedOperator Prompt, see thePrompted bindingtopic.
Provide Feedback