Binding to a material-enabled phase step
Material binding is the process of binding activated material phase steps to material-enabled equipment modules, or rebinding a previously bound material to a step within a control recipe without being prompted to do so. Material binding must be performed from within the Procedure view. The following criteria must be met to perform manual binding:
- The step is associated with a material in the recipe.
- The step is inactive or has a binding status of BINDING.
If you bind a material-based phase, you will have the opportunity to select the type of binding and/or the binding container.
- In the Batch List view, double-click the batch that requires binding.
- In the Procedure view, select the material-based phase to bind, and then click theBindcommand button. ThePrompt to Bind a Material Phase Stepopens with a list of legal binding options.

- Select the binding Lot or Storage Container for the material, and then clickOK. If there is only one option, just clickOK.
- Navigate back to the top of the unit procedure, and then click theStartcommand button; or switch to the Batch List view and start the batch.
- If you selected a specific material or Automatic, you do not need to do anything. If you selectedPrompt, aPrompt to Bind a Material Phase Stepinstruction displays in the Instructions view when it is time to select a material.
- Switch to the Instructions view, and then select the desired Lot or Storage Container from the list.

- ClickOK.
Provide Feedback