Table view
The Table view provides a list-based representation of a batch. Steps
are executed in order starting with the top row, and proceeding downward through the table.
Each row consists of an individual step and its associated information.
The following
data can be displayed:
Item | Description |
|---|---|
Name | The name of the recipe step. |
State | The current state of the recipe step. |
Mode | The current mode of the recipe step. |
Failure | The failure information associated with the recipe step. |
Unit | The name of the unit in which the recipe step is running. |
Owner | The current owner of the recipe step. |
Step Index | The current step index of the recipe step. |
Message | The message for the recipe step. |
Request | The pending request for the recipe step. |
Parameter(s) | The value of any parameters given for the recipe step. |
TIP:
Parameter values are right-justified so you may
need to scroll to the right to view them (or click the
Details
button).Provide Feedback