Edit parameter values
- Select a step of the batch.
- Click theDetailscommand button. ThePropertiesdialog box opens.
- Double-click a parameter. TheChange Parameter Valuedialog box displays the minimum, maximum, and default values of the parameter.MinimumandMaximumare blank if the parameter data type isenumeration.

- Type a new value in theValuebox and clickOK.
- ClickOKto exit thePropertiesdialog box. The selected step now displays the new value, as shown below:
TIP: The Value must be configured as the Display Parameter in the Recipe Editor (on theFormula Value Entrydialog box).
Provide Feedback