Start a material-based phase
- Acquire the appropriate phase.
- Click theStartbutton to initiate the phase. ThePhase Control Feed Type and Material Selectiondialog box opens.

- Select theFeed Type(if available), andMaterial, and then clickOK. ThePhase Controldialog box opens.

- Type a uniqueBatch IDfor the manual phase control batch in theEnter Batch IDbox, unless you are generating Batch IDs automatically.(SeeBatch identificationin thefor more information.)FactoryTalk BatchAdministrator Guide
- Select the appropriate container from theMake a selection to bind equipment modulebox and clickOK. The State changes to RUNNING.TIP: The first container on the list is the default container.
Provide Feedback