Remove a batch from the Batch List
To remove a batch from the Batch List view, selected the batch that is to be removed. The batch:
- Cannot be in MANUAL mode.
- Must be inactive. Inactive states are: STOPPED, COMPLETE, ABORTED or READY.
To remove a batch from the Batch List:
- Select the batch to remove.
- Click theRemove Batch
button.
Provide Feedback