Create a control recipe
Use
Batches
to add a control recipe from a master recipe. The Batches
list displays control recipes that are ready to run, are running, or are complete. - SelectBatches.
- SelectAdd
. - Select a master recipe.
- Enter a unique batch ID.TIP:TheBatch IDbox accepts non-unique IDs. When duplicate batch IDs are used, it is difficult to associate prompts with the correct batch when viewed in Prompts.
- (optional) Perform any of these:
- To run a batch at a percentage other than 100%, in theBatch Scalebox, enter the percentage.
- To change the description of the batch, in theDescriptionbox, enter a new description.
- If the recipe contains a material class-based phase, select the material to use in this particular batch.
- To assign or change a formula value, enter new values inFormula Values.
- Select the equipment for the control recipe in theUnit Bindingsarea. TheUnit Bindingarea appears after selecting all required parameters. By default, the equipment is not selected. The user must configure the equipment manually. A unit binding error appears if a configuration error occurs. For detailed information, selectSelect for details.
- SelectCreate
to add the control recipe to the Batcheslist.
Provide Feedback