End of batch entries
The electronic batch record (.evt or .evtj file) contains entries if the batch is terminated by a
FactoryTalk Batch
Server cold boot, or if the batch is terminated due to an error when attempting to restore the batch from a Server warm restart.The electronic batch record contains three entries if one of the above-mentioned methods for batch termination occurs. The first entry is a repeat of the Event File Name event field. The second is a System Message event field indicating the reason the batch was terminated. The last is a System Message event field indicating the end of the batch.
Example
Description | Event | PValue |
|---|---|---|
Event File Name | \\MachineName\Program Files (x86)\Rockwell Software\Batch\YourProject\ JOURNALS\4123.evtj | |
YourBatchDescription | System Message | Batch terminated by COLD boot of FactoryTalk Batch Server |
YourBatchDescription | System Message | End Of BATCH |
Description | Event | PValue |
|---|---|---|
Event File Name | \\MachineName\Program Files (x86)\Rockwell Software\Batch\YourProject\ JOURNALS\4125.evtj | |
YourBatchDescription | System Message | Batch terminated due to error attempting to restore batch during WARM restart |
YourBatchDescription | System Message | End Of BATCH |
Provide Feedback