Servers view parameters
The
Servers
view includes these parameters.The parameters are only available when online, and there is a configurable TCP or UDP server.
Parameter | Description |
|---|---|
Enable | Enables or disables the port by selecting or clearing the check box. |
Name | Displays the name of the port. |
Port | Displays the port number. |
Protocol | Displays whether the protocol is TCP or UDP. |
Refresh | Retrieves and displays the latest values from the device. |
Set | Writes pending edits to the device. Tip :
|
Provide Feedback