Loading
CASE STUDY | CHEMICAL
Recent ActivityRecent Activity

Covestro Streamlines Panel Design in Motor Starter Operations

New EtherNet/IP™ In-cabinet Solution cuts wiring time and complexity, takes up less space, improves maintainability.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Rockwell Automation EtherNet/IP™ In-cabinet Solution cuts wiring time and complexity and takes up less space.
Convestro Logo

Covestro is one of the world’s largest polymer companies, with 46 production sites worldwide that employ the latest, most cost-efficient and ecologically compatible technologies. Its business activities are focused on the manufacture of high-tech polymer materials and the development of innovative solutions for products used in our daily lives. They serve the automotive, construction, wood processing and furniture, as well as electrical, electronics, and household appliances industries and support sports and leisure, telecommunications, health and the chemical industry.

Challenge
  • Aging electrical components
  • Difficult to access system control and monitoring
  • Fluctuating ambient temperature and moist environment stressed electrical components
  • Inefficient layout of patched together motor starters
  • Limited maintenance options for 24/7 operation
Solution
  • EtherNet/IP™ In-cabinet Solution
Result
  • Over 60% reduction in wiring time for panel assembly
  • Delivered cleaner, safer and more reliable design
  • Significantly reduced project engineering and testing time
  • Layout became more accessible for preventive maintenance teams
  • Modular design can allow new devices with minimal programming

The first global adopter of Rockwell’s Ethernet/IP™ In‑cabinet Solution cut panel build time by more than half, consolidated an aging infrastructure, and improved maintainability across critical boiler and chilled water systems in its Pittsburgh polyurethane facility.

Challenge

Innovative solution was needed to reduce panel wiring time

The boiler room at Covestro’s production facility housed a patchwork of aging NEMA motor starters, scattered across seven separate enclosures with remote push buttons. Over years of continuous 24/7 operation, the extreme ambient temperatures – 80-90°F in winter and up to 120°F in summer – took a toll on electrical components, often requiring the engineering team to rely on ad‑hoc fixes to keep equipment running.

In addition, the distributed layout created maintenance complexity. Remote push buttons, long wire runs, and cluttered conduit systems contributed to downtime risk and slowed troubleshooting.

The Covestro team needed a modern, consolidated solution to build its control panels that would reduce wiring effort, simplify maintenance, and provide a cleaner, safer, more reliable infrastructure.

Solution

An improved build experience

When principal PCT engineer Chris McCartney learned about Rockwell’s new EtherNet/IP In‑Cabinet Solution, he immediately saw potential. The ability to replace large bundles of control wiring with simple ribbon cables and Ethernet connectivity promised substantial time savings and improved diagnostics.

Covestro became the first customer globally to adopt and implement the technology.

Working alongside Rockwell’s product managers and engineers, Covesto’s engineering team designed a new consolidated control panel to run:

  • Two pumps for the chilled water system
  • Five pumps for the boiler system
  • Expansion capacity for three additional pumps

The new panel replaced all seven legacy enclosures and eliminated a significant amount of outdated hardware. It also offered a safer option for a high temperature location that was at risk for flooding due to cavitation with pumps.

For Bill Polichio, Covestro’s industrial electrical technician who worked on the project, the difference was immediate and dramatic. Instead of wiring 3+ wires per push button, 2+ wires per light, remote I/O connections, and long home-run cables, he installed a single ribbon cable that linked all push buttons and indicators.

“Running that ribbon cable saved me days of work. The entire cabinet took maybe 16 hours to build, and traditionally it would have been 40 or more,” said Bill.

Even the overload wiring, usually a tedious process, was simplified to just two wires per device.

The overall build was completed in only two days, including drilling, panel layout, DIN rail installation, Panduit routing, and device mounting.

“If we can put this together, anyone can,” said Chris. “That alone makes the cost of the EtherNet/IP hardware worth it.”

his is the before picture of Covestro's motor starter layout of electrical panels at their Pittsburgh, PA facility. Using Rockwell's EtherNet/IP™ In-cabinet Solution delivered a 60% reduction in wiring timing for panel assembly and a more reliable design.
This is the after picture of Covestro's motor starter layout of electrical panels at their Pittsburgh, PA facility. Using Rockwell's EtherNet/IP™ In-cabinet Solution delivered a 60% reduction in wiring timing for panel assembly and a more reliable design.

Covestro implemented a new EtherNet/IP In‑Cabinet Solution that allowed them to replace large bundles of control wiring with simple ribbon cables and Ethernet connectivity. The new panel replaced all seven legacy enclosures, eliminated outdated hardware and provided the engineering team a 60% reduction in wiring time.

Result

A cleaner, safer, more reliable panel design

The Covestro engineering team estimated that it saved more than 60% of the time it would have taken traditionally to assemble the control panel, which would have necessitated weekend work. All pump starters were consolidated into one modern enclosure, and the innovative EtherNet/IP solution reduced wiring bulk and eliminated heat-damaged hardware. Programming was straightforward and the layout in the boiler room was made cleaner and more accessible for maintenance teams. 

Looking ahead

The modular design allows new devices to be added with minimal programming.  Covestro will also evaluate next-generation E100 electronic overload relay components, which add current monitoring, remote reset, and additional diagnostic capabilities, features the team expressed interest in for future upgrades.

Published April 22, 2026

Topics: Drive Sustainability Optimize Production Industrial Components Networks & Infrastructure Industrial Automation & Control Sustainable Solutions Sustainability Chemical Industrial Control Products
Subscribe to Rockwell Automation

Receive the latest news, thought leadership and information directly to your inbox.

Subscribe now

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Case Studies
  5. Chevron LeftChevron Left Covestro Streamlines Panel Design in Motor Starter Operations