Remove and Install the Control Pod Cover for
Frame 7

You must remove the control pod cover to access other components inside the pod. Follow these steps to remove and install the control pod cover.
  1. Review the product advisories in Before You Begin.
  2. Remove power from the system.
  3. Open the enclosure door.
  4. Loosen the two captive screws at the top of the control pod and pull the cover out from the chassis.
  5. Lift the bottom of the cover off the tabs (A) and remove the cover.
    example of how to remove the frame 7 control pod cover
    TIP: The control pod Is shown separated from the power bay to clarify the instructions only.
  6. Install the control pod cover in the reverse order of removal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal