Remove and Install the DR and PE-A (EMC and MOV) Jumper for Frame 6

Replace the DR and PE-A (EMC and MOV) jumper with kit catalog number SK-RM-JMPR1-F6. Follow these steps to remove the DR and PE-A (EMC and MOV) jumper.
  1. Review the product advisories in Before You Begin.
  2. Remove power from the system.
  3. Remove the cover from the chassis. See Remove and Install the Frame 6 Cover.
  4. Loosen the three captive, slotted-Torx head screws that secure the jumper to the power interface circuit board.
  5. Lift the jumper away from the power interface board until the keyholes in the jumper align with the pins on the sidewall and remove the jumper.
    example of the frame 6 PE-A jumper location and removal
  6. TIP: The PE-A jumper is shown in the default (IN) position.
  7. Install the DR and PE-A (EMC and MOV) jumper in the reverse order of removal.
  8. Verify that the jumper is installed in the correct position as required for your grounding scheme and application. See the PowerFlex 750-Series Products with TotalFORCE Control, Installation Instructions, publication 750-IN100, for power jumper configuration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal