Remove and Install the Stirring Fan Assembly for Frame 5

Replace a stirring fan assembly with kit catalog number SK-RM-MFAN1-F5. Follow these steps to remove and install the stirring fan assembly.
  1. Review the product advisories in Before You Begin.
  2. Remove power from the system.
  3. Remove the cover from the chassis. See Remove and Install the Frame 5 Cover.
  4. Disconnect the wire harness connector P12 from connector P1 on the fan assembly bracket.
  5. Loosen the two captive screws that secure the fan assembly to the chassis and remove the fan assembly.
    example of how to remove the frame 5 stirring fan assembly
  6. Install the stirring fan assembly in the reverse order of removal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal