View Module-level Synchronization Status
On the Synchronization Status tab of the RMCT, you can view information about all modules in the same chassis as the connected redundancy module. Use this information to identify which module pair is causing a synchronization failure. Depending on the type of synchronization failure, it can be helpful to compare the Synchronization Status tabs for the primary and secondary redundancy modules.
The Compatibility column shows Incompatible for the following reasons:
- If there is a difference between major or minor revisions of the modules
- If Front Port Crossload mode is enabled and the cable between the Ethernet ports is disconnected
Module-level Synchronization Status

Parameter | Description |
|---|---|
Slot | The slot number of the module. |
% Complete | The percentage of the synchronization status that is complete. |
Module Name | The name of the module. |
Module Revision | The firmware revision of the module. |
Secondary Readiness | The redundancy state of the module:
|
State | The state of the module’s chassis: Primary or Secondary |
Compatibility | The compatibility of the partner module in the partner chassis:
|
Provide Feedback