View the Event Log
On the Event Log tab of the RMCT, you can view a history of events for both partner redundancy modules. You can save the system event history to nonvolatile memory and export Tech Support logs to send to Technical Support.
Event Log

Parameter | Description |
|---|---|
Event No. | A unique, sequential number to identify the event. |
Time Stamp | The date and time that the event was logged. |
Event Class | A broad category to classify the event. |
Basic Info | A basic description of the event. |
Extended Info 1 Extended Info 2 | Additional information that is related to the basic description of the event. Extended information is not available for every event. |
Event Classes
The following event classes can appear in the Event Class column in the event log.
Event Class | Description |
|---|---|
Qualification Event | An event that is related to chassis qualification. For example, the qualification process succeeded. |
Disqualification Event | An event that is related to chassis disqualification. For example, the Disqualify Secondary command was issued. |
Switchover Event | An event that is related to a chassis switchover. For example, the Initiate Switchover command was issued. |
RM Fault Event | One of the redundancy modules had a major or minor fault. For recovery information, see the Code field in the fault log on the Module Info tab. See Redundancy Module Faults. |
User configuration change event | A redundancy module configuration parameter has been changed. For example, if you change the Auto-synchronization parameter from Always to Never, an event that is classified as Configuration is logged. |
Redundancy state has changed | The state of a redundancy module changed. For example, the redundancy module lost its partner. |
Chassis State Changed | The state of the redundant chassis pair changed. For example, the redundancy status changed from disqualified secondary to qualified secondary. |
Idle Qualified | An event occurred while the chassis was in an idle qualified state. The event caused the chassis to leave the idle qualified state. |
Idle Disqualified | An event occurred while the chassis was in an idle disqualified state. The event caused the chassis to leave the idle disqualified state. |
General | An event unrelated to the redundancy state or a redundancy action. |
Event Log Examples
This section contains example event log entries for typical system events.
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Switchover Event | Commanded switchover | — | — |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Disqualification Event | Commanded disqualification | — | — |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Qualification Event | Qualification succeeded | Qualification succeeded | — |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Qualification Event | Qualification Abort | Qualification aborted due to some modules not having fully compatible partners | Bitmap of compatibility assessment for modules in chassis |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Switchover Event | Redundancy Manager State: Disqualified Secondary With Primary | — | — |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Disqualification Event | Communication on switchover was lost, switchover processed with uncoordinated manner. | Switchover | — |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Disqualification Event | Qualification Abort | Qualification Abort - Primary Module Screamed on Partner | — |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Disqualification Event | Qualification Abort | Qualification Abort - Disqualify command | — |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Disqualification Event | Qualification Abort | Partner Redundancy Module has major nonrecoverable fault | — |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Disqualification Event | Qualification Abort | Qualification Abort - Module Removal | — |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Disqualification Event | Qualification Abort | Qualification Abort - Disqualify command | — |
Event Class | Basic Info | Extended Info 1 | Extended Info 2 |
|---|---|---|---|
Disqualification Event | Qualification Abort | Qualification aborted due to lack of partner RM. | — |
Provide Feedback