HMI

Depending on the network that is used to connect to HMI, plan for certain placement and configuration requirements. You can connect an HMI to a primary chassis over the
EtherNet/IP
network.
IMPORTANT:
To help prevent anomalous behavior, do not target active communication at the secondary chassis.
To communicate with HMI, the following methods are available:
  • IP address swapping—Supported by all HMI products. For more information, see IP Address Swapping.
  • Redundant controller shortcut paths—Supported by only
    FactoryTalk® View
    Site Edition with
    FactoryTalk® Linx
    software. For more information, see the High Availability Systems Reference Manual, publication HIGHAV-RM002.
The following table describes high availability system considerations for HMI on the
EtherNet/IP
network.
HMI Considerations for High Availability Systems
HMI
Considerations
  • OptixPanel
    graphic terminal
  • FactoryTalk® Optix
    software
Only IP address swapping is supported.
PanelView
Standard terminal
Same as a non-redundant system.
  • PanelView Plus
    terminal
  • VersaView® industrial computer that runs the
    Windows®
    CE operating system
Use
FactoryTalk® Linx
software, version 5.0 or later.
FactoryTalk® View
Site Edition software with
FactoryTalk® Linx
software
  • Use
    FactoryTalk® Linx
    software, version 5.0 or later.
  • Keep the HMI and both redundant chassis on the same subnet.
  • To help reduce data server recovery switchover time, consider using redundant controller shortcut paths.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal