Identify the FactoryTalk Linx RMCT Version
You must use a version of the
FactoryTalk® Linx
Redundancy Module Configuration Tool (RMCT) that is compatible with your redundancy module firmware. With FactoryTalk® Linx
, the RMCT receives compatibility information from the redundancy module firmware. If there is incompatibility, the RMCT shows only the Module Info tab and indicates the version that the firmware is compatible with.The RMCT launches at the version that is compatible with the redundancy module firmware that is installed. If you have not updated your redundancy module firmware after updating your RMCT version, the RMCT version that is indicated can differ from the updated version that you installed. You can also check the RMCT version that is installed on your computer via Control Panel.
To identify the version of the
FactoryTalk® Linx
RMCT that you have installed, follow these steps.- Right-click the title bar and choose About.The version that appears on the About dialog box is the earliest RMCT version that you need based on your bundle. The RMCT always shows the latest version that is installed. Later versions are backwards compatible with earlier versions.
Provide Feedback