Update Other Module Firmware in the New Secondary Chassis
To update firmware for other modules in the new secondary chassis, complete these steps.
- Optional: To replace module hardware, remove the module from the secondary chassis and replace it with the new module.Before you replace communication modules as part of this firmware update process, make sure that you first read Module Replacement. When replacing communication modules, the rotary switches and port configuration for the new modules must match the existing modules.
- LaunchControlFLASH Plus®software.
- Update the firmware for modules other than the redundancy module.
- Close theControlFLASH Plus®software.
- Proceed to Synchronize the Redundant Chassis Pair.
Provide Feedback