Configure the Program to Use the Fault Routine

To configure the program to use the fault routine, do the following.
  1. In the Controller Organizer, right-click the program and click Properties.
  2. On the Properties dialog box, click the Configuration tab.
  3. In the Fault field, select the fault routine.
  4. Click OK.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal