Change from a Standard to a Safety Project

Upon confirmation of a change from a standard project to a safety project, safety components are created to meet the minimum requirements for a safety project:
  • The safety task is created only if the maximum number of downloadable tasks has not been reached. The safety task is initialized with its default values.
    TIP:
    If your project already contains 32 tasks, and you try to change from standard to a safety, the project does not convert and stays as a standard project.
  • Safety components are created (such as, safety task and safety program).
  • The safety project defaults to safety level SIL 2/PLd.
  • A time-based safety network number (SNN) is generated for the local chassis.
  • A time-based safety network number (SNN) is also generated for the embedded
    EtherNet/IP
    port.
  • Standard features that are not supported by the safety project are removed from the Controller Properties dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal