Module Diagnostics Diagnostic Assembly

Module Diagnostics webpage data.
  • Instance = 32932
  • Size = 20 Bytes
Diagnostic Assembly Members
Member
Data Type
Description
IOConnections
UINT
Number of I/O connections (class 0/1).
MessagingConnections
UINT
Number of messaging connections (class 3).
MaxObservedConnections
UINT
Maximum number of observed class 3 connections.
IOCommsUtilizationActual
UINT
Represents the current I/O communications utilization for I/O traffic.
IOCommsUtilizationTheoretical
UINT
Based on information agreed during Forward Open procedure. Represents the theoretical I/O communications utilization for I/O traffic.
IOPPSActual
UDINT
I/O messages packets per second.
IOPPSTheoretical
UDINT
Based on information agreed during Forward Open procedure. The theoretical value for I/O messages packets per second.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal