Home Webpage Diagnostic Assembly

Home webpage data that provides device information and controller status.
  • Instance = 32930
  • Size = 270 Bytes
Diagnostic Assembly Members
Member
Data Type
Description
CatalogString
STRING_32
Textual catalog or model number.
ProductCode
UINT
Identification of a particular product of an individual vendor.
MajorRevision
USINT
Major revision of the module.
MinorRevision
USINT
Minor revision of the module.
CIPSerialNumber
UDINT
Serial number of device.
WarrantySerialNumber
STRING_32
Serial number of product warranty.
ManufactureDate
UINT
Date the product was manufactured.
ProjectName
STRING
Name of the project downloaded into the module.
StatusBits (Hidden)
UDINT
Summary status of device.
RunMode
BOOL
Indicates whether controller is in the run mode.
KeySwitchRemote
BOOL
Specifies whether the key is in the "remote" position.
IOForcesExist
BOOL
Indicates whether IO forces exists. It is true only when "Force" LED is amber or flashing.
IOForcesActive
BOOL
Indicates whether IO forces are enabled. Logix Designer labels it "Forces" / "No Forces". It is true only when "Force" LED is amber.
SDCardFault
BOOL
Specifies whether SD card fault appeared. It is true if SD LED is solid or flashing red.
SDCardActivity
BOOL
Specifies whether SD card is active. It is true if SD LED is solid or flashing green.
MajorFault
BOOL
A value that indicates whether the module has a major fault. It is bit 4.
MinorFault
BOOL
A value that indicates whether the module has a minor fault. It is bit 5.
IOFault
BOOL
A value that indicates whether the module has a IO fault.
EnergyStorageStatus
BOOL
From LogixDesigner this is: minor_fault_bits.10 If minor_fault_bits.10 is on, depending on the controller, the battery is low or the ESM or UPS needs to be replaced or is missing.
StatusDisplayText
STRING
Scrolling string includes:
  • Project Name
  • Ethernet Address
  • Link State (Up Down)
  • Link Speed
  • IO Fault
  • Redundancy State
MajorHardwareRevision
USINT
Major revision of the module hardware.
MinorHardwareRevision
USINT
Minor revision of the hardware module.
HardwareSeries
SINT[2]
Two ASCII characters describing the hardware series. It is Rockwell extension to the Identity object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal