Faults Diagnostic Assembly
Faults webpage data that shows major and minor faults on the controller.
IMPORTANT:
This assembly includes the structure for the DIAGNOSTICS_FAULTDETAILS user-defined data type. This data type includes the information captured for each fault. Create this UDT before you create the Fault UDTs.
Structure for the DIAGNOSTICS_FAULTDETAILS User-defined Data Type
Member | Data Type | Description |
|---|---|---|
Timestamp | ULINT | The moment when the fault occurred. It's format is the UNIX timestamp in microseconds. |
Code | UDINT | Fault code. |
Type | UDINT | Type number of the fault code. |
Description_1 | STRING | Part 1 of the fault description. |
Description_2 | STRING | Part 2 of the fault description. |
Diagnostic Faults_A Assembly
- Instance = 32934
- Size = 392 Bytes
Member | Data Type | Description |
|---|---|---|
MajorFaultsReported | UDINT | Count of all Major Faults reported |
MinorFaultsReported | UDINT | Count of all Minor Faults reported |
MajorFault1 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
MajorFault2 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
Diagnostic Faults_B Assembly
- Instance = 32935
- Size = 192 Bytes
Member | Data Type | Description |
|---|---|---|
MajorFault3 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
Diagnostic Faults_C Assembly
- Instance = 32936
- Size = 384 Bytes
Member | Data Type | Description |
|---|---|---|
MinorFault1 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
MinorFault2 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
Diagnostic Faults_D Assembly
- Instance = 32937
- Size = 384 Bytes
Member | Data Type | Description |
|---|---|---|
MinorFault3 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
MinorFault4 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
Diagnostic Faults_E Assembly
- Instance = 32938
- Size = 384 Bytes
Member | Data Type | Description |
|---|---|---|
MinorFault5 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
MinorFault6 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
Diagnostic Faults_F Assembly
- Instance = 32939
- Size = 384 Bytes
Member | Data Type | Description |
|---|---|---|
MinorFault7 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
MinorFault68 | DIAGNOSTICS_FAULTDETAILS | Fault details structure. |
Provide Feedback