Concurrent Connections Diagnostic Assembly
Concurrent Connection data information that includes Branch Failure, Failure Count, and Packets Lost.
- Instance = 32952
- Size = 12 Bytes
Member | Data Type | Description |
|---|---|---|
BranchFailure | BOOL | This attribute indicates that one or more branches towards target(s) of any concurrent connections in which this device is a participant is not open (was not opened or timed out). |
FailureCount | UDINT | This attribute is incremented every time when the Concurrent Connections Branch Failure attribute transitions from 0 to 1. |
PacketsLost | UDINT | For each concurrent connection, as long as it remains open when the consumer on the branch of concurrent connection is processing the packet, it shall subtract the last received Concurrent Connection Sequence Count on this branch from the Concurrent Connection Sequence Count of this packet. If the value exceeds positive one (+1), then that value minus one is the number of concurrent connection packets that have been lost. A concurrent connection branch timeout does not cause Concurrent Connection Packets Lost to increment. |
Provide Feedback