Set the IP Address for the Gateway
- Determine how you want to set the network IP address for the gateway: either rotary switches or a DHCP-supported method.
- Connect all supported devices to the gateway.
- Apply power to the gateway.When power is applied to the gateway:
- A network IP address based on the rotary dials or via DHCP is assigned.
- The gateway’s localEtherNet/IP™In-cabinet system IP address of 192.168.1.1 is assigned.
- Any user-defined devices on the localEtherNet/IP™In-cabinet system are assigned IP addresses in ascending order (such as 192.168.1.2, 192.168.1.3, and 192.168.1.4).
For an initial set-up of anEtherNet/IP™In-cabinet system, the gateway automatically assigns IP addresses for supported devices on the localEtherNet/IP™In-cabinet system.For a previously configuredEtherNet/IP™In-cabinet system, the gateway uses the user-defined reference topology.
Provide Feedback