Floating point denormalized

Failed to modify trend properties. A large, negative floating-point number that is greater than -1.40129845e-45 is in
Target Value
in either the
Start Trigger
or
Stop Trigger
tab. Enter a negative floating-point number no larger than -1.40129845e-45.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal