Identical Add-On Instruction

You are attempting to create an Add-On Instruction definition that matches the name and date of an Add-On Instruction definition (or data type or built-in instruction) that already exists in the project. The Add-On Instruction currently in the project will be used.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal