Select a target controller
Select a controller to use as the communications path when going online, uploading,
downloading, or opening a project. The current path appears in the
Network Browser
dialog.To select a target controller
- SelectCommunications > Network Browser.
- In theNetwork Browserdialog tree view, select the controller to use as the target device.TIP: If the device does not appear in the tree view, enter a communications driver and path manually. See Enter a communications driver and path manually.
- SelectGo Online, Upload,orDownload.
- Save the communications path:
- To save the communications path as the current path, clickApply.
- To save the current path to the open project file, select theApply to Current Projectbox and then selectApply.
Provide Feedback