Network Browser dialog

The
Network Browser
dialog displays network topologies and contains configuration options for FactoryTalk Linx software which supports communication with devices. FactoryTalk Linx communication software is included with the Logix Designer application.
Use the
Network Browser
dialog to perform the following tasks:
TIP: To open the
Network Browser
dialog:
  • Select
    Communications > Network Browser
    .
  • Navigate network topologies
  • Select, modify, or clear the path that
    Logix Designer
    uses when a
    Go Online
    ,
    Upload
    , or
    Download
    command is initiated.
  • Download a project from
    Logix Designer
    to a controller
  • Upload a project from a controller to
    Logix Designer
  • Update firmware to a controller
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal