Rename SFC Element command
Choose this command to edit the name of the selected sequential function chart language element.
TIP:
If you choose this option, you are changing the name of the tag associated with the current SFC language element. If you double click the language element, however, and press Enter on the name field to edit that field, you are associating that language element with a different tag.
Provide Feedback