Module Properties - RSNetWorx for EtherNet/IP
Use this tab to:
- launch RSNetWorx for EtherNet/IP to view and/or edit the respective network
- associate a EtherNet/IP project file with the respective module
- audit an EtherNet/IP network
Parameters
EtherNet/IP File (.enet)
Displays the name of the EtherNet/IP file you want to associate with the module. By default, this field is blank.
Browse
Click this button to search for the file you want to associate with the module.
Found In
Displays the location where the network file was found. If no file was found, this field does not appear on the dialog.
Launch RSNetWorx for EtherNet/IP buttonClick this button to launch RSNetWorx for EtherNet/IP, from which you can:
- view and/or edit the network
- audit an EtherNet/IP network
For EtherNet/IP networks, this button is not enabled until:
- you have specified an EtherNet/IP project file, and
- you have specified an IP address or host name for the EtherNet/IP scanner
You must also apply any pending edits before you can launch RSNetWorx.
Status
Displays the status the controller has about the module:
This status: | Indicates: |
Standby | a transient state that occurs when shutting down |
Faulted | the controller is unable to communicate with the module When the status is Faulted, the Connection tab displays the fault. |
Validating | a transient state that occurs before connecting to the module |
Connecting | a state that occurs while the connection(s) are being established to the module |
Running | the module is communicating and everything is working as expected |
Shutting Down | the connections are closing |
Inhibited | the connection to the module is inhibited |
Waiting | a connection to this module has not yet been made due to one of the following:
|
Offline | you are not online |
OK
Click this button to accept your edits on any tab and close the dialog.
Cancel
Click this button to cancel your edits on any tab and close the dialog.
Apply
Click this button to apply your edits on any tab and continue editing.
Help
Click this button for help on this tab.
Provide Feedback