Menu Access to RSNetWorx Software

For ControlNet modules
Right-click the module and select
Launch RSNetWorx
. RSNetWorx software is used to:
  • Save the current network data into the ControlNet project file (*.xc).
  • View and edit the network.
  • Schedule a ControlNet network.
You must apply any pending edits before you can launch RSNetWorx  software for ControlNet.
This option is not enabled until:
  • You have specified a ControlNet project file.
  • You have specified a slot number and a node number for the ControlNet scanner.
For DeviceNet modules
Right-click the module and select
Launch RSNetWorx
. RSNetWorx  software is used to:
  • Save the current network data into the DeviceNet file (*.dnt).
  • View and edit the DeviceNet network.
This option is not enabled until:
  • You have specified a DeviceNet project file
  • You have specified a slot number for the DeviceNet scanner
For EtherNet/IP modules
Right-click the module and select
Launch RSNetWorx
. RSNetWorx software is used to:
  • View and edit the network.
  • Audit an EtherNet/IP network.
You must apply any pending edits on the profile before you can launch RSNetWorx.
This option is not enabled until:
  • You have specified a valid EtherNet/IP project file
  • You have entered an IP address or host name for the EtherNet/IP scanner
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal