Download
After a program is created in Logix Designer it must be transferred from the computer to
the controller.
- Upload - Transfers the program from the controller to the computer.
- Download - Transfers the program from the computer to the controller.
Performing this task uses these items:
Item | Description |
---|---|
Communications tree | A hierarchical representation of a network topology that is rooted at a specific server host device. |
Network Browser | The tool to navigate network topologies and configure software that supports
communication with devices. FactoryTalk Linx communication
software is included with Studio 5000 Logix Designer. To configure it, navigate to
Communications > Network Browser . |
Communication Path | This is the CIP path that identifies the communications drive, the device address, and port. It is used by Studio 5000 Logix Designer when executing a Go Online, Upload, or Download command. |
Program mode | The controller mode during which logic is not executing, outputs are not controlled, and editing operations are available. If the keyswitch is in Remote, the controller is in Remote Program mode. |
To download a program
- SelectCommunications > Network Browser.The communication software launches in theNetwork Browserdialog and displays the communications tree.
- Select a controller from the tree.
- SelectSet Project Pathto always use this communications path with this project.
- SelectDownload.Confirm the download procedure. Since the communications path is configured, the download works immediately, and the project is downloaded to the controller. Download status and compiler messages appear in the status bar.TIP: The controller must be in Program mode or Remote Program mode before downloading the project.
Provide Feedback